Other Parts Discussed in Thread: DRV8816,
Hi Team,
May we ask your help regarding the customer's inquiry below.
I'm looking for a driver for 8 24V push-pull outputs.
In the past I´ve also used the DRV8816 if I need two outputs.
But the DRV890x family is so described from the perspective of a motor driver, I am not sure if I have overlooked something that contradicts the individual use of the outputs.
PWM ->OFF
enable extended overvoltage
OLP: (OLD_OP = 1 and OLD_REP = 1 ) OR all HBx_OLD_DIS=1
...
I am not sure whether I have captured all the boundary conditions with it.
Have I missed something?
Regards,
Danilo