if R62,R68,C52 & R73,R77,C61 can be removed?
Can DRV8705-Q1 detect motor status?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
if R62,R68,C52 & R73,R77,C61 can be removed?
Can DRV8705-Q1 detect motor status?
Hi Zhengwei,
If by motor status you mean motor current then yes. As long as R79 is included and connected to SN and SP, the motor current can be monitored through the SO pin.