Hi,
We are in need to control 4 or 8 solenoids with 24V@500mA rating. I have found this part DRV8932PPWPR which well suits our application. However i have some confusion over controlling the 4 inputs.
In datasheet, its mentioned to use PWM pin for controlling the 4 inputs but instead I want to control them through GPIO as Software complexity reduces while driving through GPIO. In my application, i need to turn ON and OFF solenoid frequently(every 400ms) and hence i don't want to go with PWM approach.
Hence i want to know if Logic GPIO control can be used for the purpose. Datasheet specifies about logic control but its not clear as all the waveforms given are related to PWM control.
Regards
Kumar