Other Parts Discussed in Thread: DRV8906-Q1
Hi team,
Is there no issue by on its resistance variation with half bridge parallel connection?
I would like to use a 3A peak motor load with some of other loads such as LED or additional motors.
DRV8912-Q1 datasheet says it could deal with 3A by operating multiple half bridge in parallel for current dividing. Then I am worried about on resistance variation. Is there any care points to use this operation to deal with high load motor by DRV8912-Q1?
Regards,
Ochi