Other Parts Discussed in Thread: DRV8702-Q1, , DRV8711
Dear Community,
we are planning a driver for fast switching 2 solenoids.
Currenlty planned spec is 48V/4A with long term perspective of 60V/6A
Must Have:
- Boost with Currentlimit
- Reverse Polarity for fast decay
- Current regulated Hold Phase
So I was looking at DRV8702-Q1 and its current sensing output S0, but its lacking a higher solenoid voltage.
I took a look at DRV8412 which is suitable but for current regulation in Hold phase a separate current detection would be necessary.
I guess it would be better to have a controller plus external Mosfets and Boost current sensing. And a separate current sensing for the adjustable hold current?
Any tips or suggestions are welcome!
Thank you.