Hi team,
Our customer asked some questions to DRV8714S-Q1. Please answer the following questions.
(1) Customer thinks to connects some of DRV8714S-Q1 pins to GND. DRV8714S-Q1 has some type of GNDs which are AGND, PGND and DGND, so could you tell me which GNDs should these pins connect to?
5pin: IN2/PH1
6pin: IN3/EN2
9pin: DRVOFF/nFLT
10pin: AREF
12pin: SO1
13pin: SO2
14pin: BRAKE
15pin: SP1
32pin: GND
(2) Customer thinks to control 2 DRV8714S-Q1 by 1 MCU. Can customer connect DRVOFF/nFLT and nSLEEP pins like the following configuration?
Regards,
Nishimura