I am interested in utilizing the DRV110EVM evaluation board to drive a +24VDC solenoid at an initial peak current of 533 mA before dropping its sustained current to 267 mA. With the use of external resistors the DRV110EVM board has a max hold current of 150 mA which is unfortunately too low. Therefore, an external FET would be required with the DRV110EVM to drive the current load and the DRV110EVM would serve to control step current level such as .533A/0.267A.
Would it be possible to get some feedback on this external FET setup to achieve these specifications?