This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-DRV8320H: motorVars.VdcBus_V parameters is always display 2.1V

Part Number: BOOSTXL-DRV8320H
Other Parts Discussed in Thread: LAUNCHXL-F280049C, BOOSTXL-DRV8320RS

Hi there,

I'm running example 5(motor_id_out) from the C2000_MotorSDK using LAUNCHXL-F280049C with BOOSTXL-DRV8320H. While running on CCS real-time debugging, in expression window  motorVars.VdcBus_V is showing 2.1V. I connected a BLDC hub motor with 48V supply. There is no lose connection. What could be the issue. Is it a issue related to DRV8320H while code is for DRV8320RS?