Hi Support team
Does DRV2700 supporting following conditions, if no, do we have suitable one?
INPUT Signal: INPUT: SINE WAVE 200KHz, +/- 5 V PIEZO AMPLIFIER (magnification x10 to x100) output +/- 50V
PZT Load: 3nF
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Support team
Does DRV2700 supporting following conditions, if no, do we have suitable one?
INPUT Signal: INPUT: SINE WAVE 200KHz, +/- 5 V PIEZO AMPLIFIER (magnification x10 to x100) output +/- 50V
PZT Load: 3nF
Hello,
The DRV2700 does not really have bandwidth larger than 20kHz max, even for such a small load.
The best path forward would be to look through TI amps and look for ones that have such a large bandwidth and can also handle a 3nF load.
Best regards,
Carson
Low Power Audio Applications