Dear Teams,
My customer is using DRV8353. When they toggle the enable signal, such as change from enable to disable or reverse, they found the output voltage sometimes is 1.5V, sometimes will be 1.51V. They set the ref voltage to 3V without any changes. Could you help give some suggestions why output voltage sometimes will go to 1.51V? The probability of 1.51V event occur is around 10%. You can find the schematic diagram here:
Thanks!
Dylan