Other Parts Discussed in Thread: LMG1210, INA280, UCC27282, DRV835X, ABS
Hi all
Our customer wants to implement a BLDC running at 100V.
I assume they cannot use the DRV8353 as they would need some safety margin vs. the max operating voltage of the device.
Is my assumption correct ?
Do you have other suggestions ?
They are looking also at a discrete implementation, e.g. with LMG1210 and INA280, however this will be expensive.
I also suggested the UCC27282 but they have only one PWM-signal to control the driver, therefore the UCC27282 is not compatible with their control interface.
Best regards
Ueli