Hi experts,
Customer will use 1.8V pulse for control input. I think it is ok since above 1.45V with the situation 1.65V<VM<11V in 7.5 Electrical Characteristics.
I would like to make sure 1.8V logic high is ok for 3.3V VM, correct?
Regards,
Hideki