This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10964: Efficiency tuning using align the motor’s phase current

Part Number: DRV10964
Other Parts Discussed in Thread: DRV10963,

Dear team, 

Is there any way tuning to align the motor's phase current to improve efficiency? 

In case of DRV10963, there is Control Advance Angle function but the DRV10964 is fixed type. is it right?

To improve efficiency of DRV10964, Is there any way of tuning DRV10964 angle using external circuit or layout? 

Thank you.