Hello,
I have just received the evaluation board for the MCT8316Z. The good news is that I was able to connect a sample of the Maxon motor we are planning to use and it seems to function as expected. One question is regarding the RPM calculated by the Evaluation Web application. The FG_OUT frequency read by the application matches what I see on a scope, but the RPM calculated by the application is about 10X larger than actual. So, for example, when the FG_OUT is 57Hz, the application displays an RPM value of 1663 RPM when the motor is spinning about one tenth that speed. In this case, the motor is slow enough that I can count about 3 rotations per second which would be somewhere around 180 RPM. This Maxon motor has 4 pole pairs and I have selected 4 pole pairs in the application. Please let me know if this is a known bug or if there is something else I need to set in the application to get it to display the correct rotational speed.
Thank you,
Randy Holmberg