Other Parts Discussed in Thread: UCC27282,
The customer would like to know if UCC27282 is suitable for use as a brushless permanent magnet synchronous servo motor.
Some basic information about the motor is as follows:
Continuous current: ADC--12.00 Arms--10.00
Peak current: ADC--40.00 Arms--30.00
Rated Continuous Output Power: Watts--350
Speed at Rated Power: RPM--2400
Design Voltage: Vbus--48.0 (Vdc) VAC--34 (Vrms)
Back EMF: Vpk / kRPM- 18.5 Vrms/kRPM--13.0
Motor constant: N-m/ √ watt--0.28 Oz-in/ √ watt--39.5
Inductance: LM--0.55
Thanks!
Best Regards,
Cherry Zhou