This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353R: UCC27282 select comparison

Part Number: DRV8353R
Other Parts Discussed in Thread: UCC27282,

The customer would like to know if UCC27282 is suitable for use as a brushless permanent magnet synchronous servo motor.

Some basic information about the motor is as follows:

Continuous current: ADC--12.00 Arms--10.00

Peak current: ADC--40.00 Arms--30.00

Rated Continuous Output Power: Watts--350

Speed at Rated Power: RPM--2400

Design Voltage: Vbus--48.0 (Vdc) VAC--34 (Vrms)

Back EMF: Vpk / kRPM- 18.5 Vrms/kRPM--13.0

Motor constant: N-m/ √ watt--0.28 Oz-in/ √ watt--39.5

Inductance: LM--0.55

Thanks!

Best Regards,

Cherry Zhou