Due to the U.S. Thanksgiving holiday, please expect delayed responses during the week of 11/22.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8316A: MCF8316A/MCT8316A/MCT8316Z RTM Schedule

Part Number: MCF8316A
Other Parts Discussed in Thread: MCT8316Z, MCT8316A

Hello Sir/Ms.

I saw that samples of these ICs (MCF8316A/MCT8316A/MCT8316Z) are ready for application. According to previous experience, there are samples that can be applied for, which means that it is about to be mass-produced. May I know when the mass production time is?

I have customer needs 24V/2A BLDC analog control. I would like to recommend these Motor Driver ICs.

Best Regards,

Kami Huang