Hi team.
What's the difference between DRV10983 and DRV10983-Q1? Can you summarize a comparison table? Can I replace DRV10983 with DRV10983-Q1 directly without changing the hardware and software?
Br,
Nison
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team.
What's the difference between DRV10983 and DRV10983-Q1? Can you summarize a comparison table? Can I replace DRV10983 with DRV10983-Q1 directly without changing the hardware and software?
Br,
Nison
Hi Nison,
We will provide you a formalized response on Monday.
Thanks,
Aaron
Hello Nison,
Thanks for posting to the MD forum. The DRV10983 and DRV10983-Q1 are pin to pin compatible and operating temperature is the same, so you may use as a hardware drop-in replacement. There are a couple of small differences between the devices but are some bigger which still make the devices compatible for replacement:
Device | DRV10983 | DRV10983-Q1 |
Supply (Min) | 8V | 6.2V |
Supply (Max) | 30V | 45V |
As far as software goes, the register maps between the two devices is not identical so there are firmware changes that would need to be made if you are looking to replace a DRV10983 with the DRV10983-Q1.
Best,
Isaac