Other Parts Discussed in Thread: MCT8316Z, MCT8316A, , DRV10987, DRV10970, TLC555
Hello Sir/Ms.
My customer used architecture MC33039+MC33035 before.
Hope to find an alternative. Can replace the existing structure.
His motor specification is
3-phase BLDC with Hall sensor input
Voltage 24V@ 2A,
Speed control method: Analog input (0~5V), PWM two kinds
Positive and negative control is possible,
Can brake
I have introduced MCT8316Z, MCT8316A and MCF8316A. MCT8316Z has no analog input. MCF8316A and MCT8316A do not have RTM yet.
Is there any suitable Device I can introduce?
Best Regards,
Kami Huang