Part Number: DRV8432
hi,
I'm using DRV8432 to drive TEC-XLT2418, the flow chart is below
1. heat TEc to 90℃ by PWMing PWM_A(buty cycle 100%) and PWM_B(buty cycle 0%),
2. then cooling it down by PWMing PWM_B 100%(buty cycle 100%) and PWM_A(buty cycle 0%)
but we found one question, at the moment of cooling down from 90℃, the TEC+ is still high while PWM_A is 0%, and hold up 1s above.
why it happened? when PWM_A low, why TEC+ can't drop down to low instantaneously with PWM_A?
the design is below.
BR
Jerry