Other Parts Discussed in Thread: MCT8316A, , MOTORWARE
Hi experts,
My customer wants to know the maximum RPM that can be controlled by MCF8316A and MCT8316A.
Their motor parameters are:
- VM : 12V
- R : 0.42ohm
- Lq=Ld: 0.2uH
- BEMF : 1.324mV/Hz
In the case of InstaSPIN of C2000, I was able to know the maximum RPM that can be controlled by the following Excel(motorware_selecting_user_variables.xlsx).
I want to know how to calculate the maximum RPM with MCx8316A.
Best regards,
Sasaki