Other Parts Discussed in Thread: LMD18201
LMD18200/NOPB in short supply.
LMD18201/NOPB is available.
My design does not use the current sense pin. Can I use LMD18201 in place of LMD18200?
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LMD18200 has pin 8 connected to 2.2K resistor (0.1 uF capacitor is in parallel with the resistor).
Where can we find LMD18200?
If I use 0-ohm resistor to replace 2.2K resistor on pin 8 of LMD18200, can I use LMD18201? Or the performance is not comparable?
Pragnesh,
If you don't need the current sensing output from LMD18200, yes, you can use 0-ohm resistor to put pin 8 to ground and use LMD18201.
Regards,
Wang Li