This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8881: XVREF's Recommended Operating Conditions

Part Number: DRV8881


Hi All,

I have a question on DRV8881.

The maximum recommended operating range of VREF is V3P3,
If the output of V3P3 is 2.9V, is it a rating violation if 3.6V is input to VREF?

Or is VREF capable of inputting up to 3.6V regardless of the output of V3P3?


Best Regards,
Ishiwata