Hi I think my board has failed. I was running the motor with a supply of 20V 20A cutoff. Motor had min load and was running at 1.6A. Wanted to check the function of DRV/OFF and SLEEP. When I turned off by switching using sleep, it worked fine for a couple of times, then ceased to work. Now there is no control of the motor at all. It is always on, with PWM at 0 and INHiz at low. I have disconnected the 0 ohm resistors to these pins for use with external PWM so know these are at zero. GH1 and SH1 are both at PVDD. I cannot reconnect the GUI. Was working fine till I turned on and off via sleep a couple of times. The lights Status PVDD and DVDD are good. n fault comes on briefly on shutdown, was overvolt, but can not see now!
Bothered as by this am planning to use this for a Greenpower F24car (have my own layout with much larger MOSFETS). A full on mode failure is something that I cannot allow to happen ....
Please can you advise