This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8350H-EVM: Sensored Firmware loaded and GUI recognizes that, still cannot get motor to spin getting MCU faults with default settings

Part Number: DRV8350H-EVM
Other Parts Discussed in Thread: DRV8350,

I believe I have everything set up to properly spin a sensored motor using the EVM board but, I keep getting MCU faults and I do not see why.

I have the Dev board hardware reworked with the following to work with sensored Firmware

  • Hall sensors resistors R46, R48 & R51 = 0 ohm
  • J1 jumped to 5V0 (for 5V hall sensors)

The Sensored Firmware has also had the INCLUDES and the typos in init.c fixed is installed and the DRV835X-EVM GUI recognizes this Firmware by only allowing me to select sensored.

I am not sure if there are any other hardware changes or settings that I need to change to get the Dev board up and running to actually evaluate the DRV8350's performance.