Other Parts Discussed in Thread: DRV8350, MOTORWARE
Hello!
I am trying to drive a Maxon Brushless DC Motor with the DRV8350H-EVM and the DRV8350X-EVM GUI. I have been trying to run the motor with 1x-PWM mode (I removed R66 to set this). With the current limit set to 35A, no matter how I set the remaining settings, I can only get the motor to begin the turn on procedure (I think this is the initial position detection) before the MCU fault light on the board turns on and an "Unknown Fault" error shows on the GUI. I am looking for help as to how to set up the GUI in order to have the motor spin. Any advice helps!
Below are specs for the motor.