Hi team,
Issue: Is it okay to pull up the RD to 3.3 V? Or it can only connect to V5 or VCC (12V) ? The specification states that the pin is open-drain, although it is pulled up to V5 or VCC. So is the open drain output 3.3V OK?
Could you help resolve this case? Thanks.
Best Regards,
Cherry