The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8834: Motor voltage clamping

Part Number: DRV8834

Hi, I'm using DRV8834 to drive a small stepper motor to open/close an air vent. If a user manually opens the vent, we think the backdrive may be causing a small number of field failures as the energy from the manually rotated motor gets fed back to the driver. The o-scope screenshot below shows one of the motor outputs, which appears to be clamping at ~5.8V. The clamping only appears to occur when the driver is in sleep mode. Our plan to fix this is to add some bulk capacitance to the motor rail, but I want to make sure we understand the problem.

Channel 1:  Motor output

Channel 2:  Motor power supply 

Does it look like the internal MOSFET or some internal protection component is going into breakdown (does 5.8V clamping make sense in this context)?

Thanks!

  • Hello, Elaina:

    1. The voltage is generate by the vent motor which is related to the motor speed. 

    2. When a user manually opens the vent, the input bus is the load. DRV8834 is a 11V device. I don't think it clamps the voltage at 5.8V. Before add more input capacitor to clamp it, I would add a resistor at input to see how many energy is sent back. And then, according to the energy (1/2*C(V1)^2-1/2C(V2)^2) to calculate the input capacitor.

    3. The clamping only appears to occur when the driver is in sleep mode. Yes. In brake mode, the energy will be burned out in the low side FET and motor coil.

    Regards,

    Wang Li

  • Thank you very much for answering my questions.  The issue turned out to be the buck regulator chosen.  The over voltage protection of the buck supply was kicking in and clamping it at the 5.7V.  I appreciate your response.  It assisted with eliminating the driver as the problem.