This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2625EVM-CT: Motor drivers forum

Part Number: DRV2625EVM-CT
Other Parts Discussed in Thread: DRV2625EVM-MINI, DRV2625

Hello,

I am using the DRV2525EVM-CT to evaluate an external LRA device.
I would like to set the LRA device inside the enclosure and evaluate it using I2C communication from outside, but I need to press and hold the + button once to change the DRV2625EVM-CT to I2C mode.
If possible, I would like to change to I2C mode automatically when I turn on the DRV2625EVM-CT. Is there a good way to do this?

Best regards.

Taku