Other Parts Discussed in Thread: DRV2700
Hi Team,
We want to design a piezo blower driver.
Our requirements are as follows
Our input voltage is 3.7V nominal (2.8V to 4.2V).
The required output voltage is 60V AC.
The maximum continuous power of the blower is 1.2W.
The snippet from the datasheet of the blower is attached here.
We want to adjust the voltage to the piezo blower using the DAC of the MCU by voltage injunction at the FB pin. Is this [possible with this IC?.
Or can I adjust the output voltage through I2C?.
The AC drive required for the blower is 20-22KHz.
Is the IC DRV2665RGPRgood for our application?.
Please suggest one if this is not suitable for our application.
Looking forward to hearing from you.