Other Parts Discussed in Thread: DRV8434SEVM
Hello All,
I have DRV8434SEVM and I want to test this with my microcontroller.
1) I have removed resistors around j3 jumper and connected
2) GND and VCC (3.3) from my microcontroller Board.
3) SDI, SDO, nSCS and SCLK with SPI of my board.
4) I have shorted nSleep, Enable, vsdo, vref with 3.3 volt.
5) nFault i have pulled up via 10kohm.
6) vbat i have connected to 24 volt.
I am missing anything?
Question: If i do not connect USB to this eval board and then if i do not connect 3.3 volt from microcontroller, then also at J3 connector, on 3.3 v pin, I am getting voltage.
if you have some other source code and setup example, kindly share
Thanks
Sudhanshu