This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8304: DRV8304S vs DRV8323S

Part Number: DRV8304

Hi there,

What are the differences between DRV8304S and DRV8323S?

Are they fully p2p compatible? Software compatible?

Our application is a 24V 200W BLDC.

  • Hi Daniel,

    These devices are P2P compatible. Differences are that:

    • These devices have different heights and thermals 
    • DRV8304S is recommended for 12-V systems, abs max 40V
      • Smaller max IDRIVE settings (300mA peak sink current)
    • DRV8323S is recommended for 12-V or 24-V systems, abs max 60V
      • Higher max IDRIVE settings (2A peak sink current)

    Thanks,
    Aaron