This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8701: Motor Voltage

Part Number: DRV8701
Other Parts Discussed in Thread: DRV8874

Hi,

I am planning to use 7.2V motor with DRV8701.

The datasheet mentions "The DRV8701 is a single H-bridge gate driver that uses four external N-channel MOSFETs targeted to drive a 12-V to 24-V bidirectional brushed DC motor."

But the operating voltage is between 5.9V to 45V.

Can you please clarify?

If DRV8701 is not suitable, is there an alternative with external FET to drive 7.2V motor