Hi, TI Support Team
Please inquire for detailed product features.
Because it is difficult to check the reference circuit diagram through the datasheet,
Please share data other than the datasheet.
Please answer the following questions.
1. I know that overcurrent setting is possible when overcurrent is detected. Is it necessary to use SPI communication when setting? HW Is there anything to be added separately?
2. Is it possible to detect a motor short circuit?
3. Is PWM control possible? (MOTOR SOFT START function required.)
4. You want to use 2 products. Is individual control possible for each motor?
5. nSLEEP function will not be used. How do I process PIN? (MCU power is off when the product is not in operation.)
- In the case of OPEN, is there any possibility that CURRENT will flow through the corresponding port?
6. If MCU available ports are limited and you need to use 2 DRV8245-Q1, is there a pin that can be used in common?
If you have a shared PIN, how do you configure it?
7. There are HW Variant and SPI(S),(P) methods. What is the appropriate method for applying the above functions?
Thanks.
Regards,
MJ