Other Parts Discussed in Thread: DRV8323
Hello,
I am evaluating the BOOSTXL-DRV8323RS andI wanted to ask about TDRIVE and dead time specifics. Take a look at this scope shot:
CH1: Motor Phase A Current, CH2: nFAULT, CH3: GHA, CH4: GLA

I set the IDRIVE settings to the lowest and TDRIVE to the lowest (500ns) to see if I can trigger gate drive faults. In the above scope shot it takes 1.1us to properly go LOW which should trigger the fault. However, upon rereading the TDRIVE section of the DRV8323 datasheet again, it seems that the t_drive is measured between some unknown pair of Vgs thresholds.
Where can I find these thresholds?
These unknown thresholds could also explain why there is overlap between GHA and GLA in the above scope shot, despite there being a supposed dead time insertion.
Jerome