Hi Experts,
When DRV8874-Q1 is working as direct drive forward-rotating. High side OUT1 short to GND. The nFAULT was driven LOW. What can trigger nFAULT LOW?
According to the fault condition,
- The current mirror is on low side, so it can't be trigger by OCP or Itrip.
- The test Vm is close VBATT, far above UVLO, so it can't be trigger by UV.
- The nFault can be trigger as soon as short, so it can't be trigger by TSD.
What else reason can trigger this?
BR
Frank