Other Parts Discussed in Thread: DRV10983
Hello everybody,
I'm facing a problem with DRV10983-Evalboard:
Started with Board No. 1:
Connected all needed wires and checked connections and polarity to make sure nothing goes wrong when powering up (24Vdc from linear PSU).
When plugging in 24V the Current Limit of the PSU comes up and stays a 3 Amps. After checking the three Halfbridges of the DRV10983 it showed up that four of six Mosfets are shorted.
Changed Eval-Board
Started with Board No. 2:
Connected all needed wires and double checked connections and polarity to make sure nothing goes wrong again when powering up (24Vdc from linear PSU).
No current limiting and smoke when powering up. BLDC tried to turn and stopped. Disconnected 24V made some checks and powered up again.
Same damage as on Board No.1, after checking the three Halfbridges of the DRV10983 it showed up that four of six Mosfets are shorted.
Any ideas what could cause this problem?
Best regards
Frank