Hi support team.
My customer has asked to me regarding VM voltage ramp.
What is the risk if the absolute maximum rating (4V / us) of the VM's voltage ramp rate is exceeded?
Thanks and Best Regards,
Higa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi support team.
My customer has asked to me regarding VM voltage ramp.
What is the risk if the absolute maximum rating (4V / us) of the VM's voltage ramp rate is exceeded?
Thanks and Best Regards,
Higa
Hi Higa-san,
We need to check with systems and design to see why this spec is implemented. We will get you a reply by the end of the week.
Thanks,
Aaron
Hi Higa-san,
There is an ESD diode from VCP-VM in the DRV8316. VM slew rates faster than 4 V/us can exceed the ESD rating and cause the ESD diode to damage and fail. This value is also spec'd from simulations so that design blocks do not behave unexpectedly (unintentional turn on of transistors), or else this can cause damage the device in some cases.
Thanks,
Aaron
Hi Aaron-san
Thank you for answering.
My understanding is that the device is damaged by latch-up if VM ramp rate is exceeded, is correct?
Best Regards,
Higa
Hi Higa-san,
If the VM ramp rate is exceeded there can be some current paths in the device that may begin to conduct, which can possibly lead to damage to the device. As long as the customer operates within the VM ramp rate specifications of the datasheet that should prevent any such issues.
Regards,
Anthony Lodi