Hello BLDC team:
I have some questions about "No motor fault" of DRV10975,Pealse help me to confirm.
When I config the "no motor fault" enable ,the motor will startup fail at sometimes(the motor in the hot condition,Ambient temperature is about 60°C) .And when I config the "no motor fault" disable,the motor can startup at all the time.All config and condition environments are the same,except the config of "No motor fault”.
About no motor fault description in the SEPC is like this:The phase U current is checked after transitioning from open loop to closed loop. If phase U current is not greater than 140 mA then the no motor fault is treated and reported as a fault.
So ,my question is:
1.Is the no motor detect always available? Including open loop、the moment of transitioning from open loop to closed loop、 the closed loop?
2.140mA is RMS or the peak value of phase U? I reduce the speed of the motor in closed loop and abserve the current of phae U with oscilloscope,when the vaule(Rms and max) are less than 140mA,there is no fault reported ,and motor can work normally.Also I config the "no motor fault" enable.
3.Lock detect schemes like the following picture,No motor fault use the dotted line,is different from the others?
Looking forward to your reply.
Best Regards!
Chris