Hi there,
In my pcb, which uses MCT8316Z spi version, along with a stm32g0 controller; I am getting NPOR bit set (error) while register read in the starting and hence the n-Fault pin is getting set and hence I am unable to drive the motor as well.
I have physically verified the voltage at the VM pin of MCT, and it is coming as it should be (24 V in my case), but still it is giving same error.
Any idea of what might cause this issue will be helpful.
Thank you.