Hello,
In simulation of DRV8304 motor driver on Pspice for TI.
Below are some sanpshots of circuit and error.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
In simulation of DRV8304 motor driver on Pspice for TI.
Below are some sanpshots of circuit and error.
Hi Subhashish,
Can you try setting the IDRIVE settings in the DRV8304 SYMBOL PARAMS to settings that are within the DRV8304 electrical specs?
It may be encountering a behavioral model issue if the IDRIVE_xPSx_ parameter is out of bounds of the definition of the DRV8304 IDRIVE settings (150mA source/300mA sink peak gate drive current).
Thanks,
Aaron
Hello Aaron,
I have changed the IDRIVE setting according to the datasheet of DRV8304 which is shown below in attached snapshot. But same error is showing again.
Hi Subhashish,
Today was a TI holiday in the US, so we will try to respond some time this week.
Regards,
Anthony Lodi
Hi Subhashish,
I need time to look into this with our PSPICE experts. Can I provide an update by the end of the week?
Thanks,
Aaron
Hello Aaron,
The view symbol present in "pspice for TI" has 11 ports. But in Pspice Model (code) of the device has only 10 ports described.
So I download the Pspice Model from ti.com (design & tools simulation of DRV8304) and that worked for me.
Thanks
Subhashish Anand