Hi,
I just got a DRV8353RS-EVM and use TI GUI(1.0.0) to control a PMSM. VM is 24V. No SW involve.
I can see the motor idenfifcaiton . then the motor can spin and I can control its speed. but I just noticed the nfault led is keep blinking. and the fault is VDS_OCP ( BTW, Occasionally, VDS_HC fault can see. I don't know why?)
so, I tried to set the VDS_OCP threshold from 0.06 V and 2 V, but still can't stop reporting this issue. and the nfault led keep blinking. would you please suggest if anything wrong here? thanks.