Other Parts Discussed in Thread: DRV10975,
Hello TI experts,
I am trying to using DRV10983EVM to spin my fan in hand. The fan looks rotating well, but the phase current is not so good i think.
I tried to tuning according to the "DRV10983 and DRV10975 Tuning Guide" (SLOU395D), the motor parameter is as below:
OPERATION VOLTAGE |
NUMBER OF POLES |
MAXIMUM SPEED(RPM) |
MAXIMUM CURRENT |
R (PHASE-CT) |
Kt (PHASEPHASE) |
LR CONSTANT |
INERTIAL |
24V |
2 |
--- |
0.35mA |
1.35OHM |
20mV/Hz |
26.59mA |
200ms |
here is the register value:
"DRV10983 0x20 0x49""DRV10983 0x21 0x1B"
"DRV10983 0x22 0x2"
"DRV10983 0x23 0x0"
"DRV10983 0x24 0x40"
"DRV10983 0x25 0xFD"
"DRV10983 0x26 0x93"
"DRV10983 0x27 0xB0"
"DRV10983 0x28 0xFF"
"DRV10983 0x29 0xF9"
"DRV10983 0x2A 0xD"
"DRV10983 0x2B 0xC"
the current curve in Tuning Guide should be sinusoidal as below:
How can I tuning the fan to get the good current wave? thanks!