Hi team,
Here's an issue from the customer may need your help:
In slow decay mode, high and low (no PWM) motor commutation occurs when the motor current is pulsed high before entering the chopping current platform, but no high pulsed current occurs in fast decay mode. Motor VM 24V, 0.5A running current. The chopping current value is set at 4 A.
The following figure shows the slow decay mode current waveform with high pulsed current. Chopping does not start, but start until after a period of time. Why is this?

Could you help check this case? Thanks.
Best Regards,
Cherry