Other Parts Discussed in Thread: DRV8426E, DRV8424, DRV8428
Hi,
Our customer is considering using the following products:
・DRV8848
・DRV8426E
・DRV8424
・DRV8428
And customer want information on what percentage of the output current error will be under the following conditions:
・ Input voltage range: 10.3V to 13.1V
・ Set current value: 300mA
・ Specifications Environmental temperature: -15 ℃ ~ 55 ℃
■Is it possible to provide the data of output current error (ΔItrip)?
Best Regards,
Nishie