Hi,
We are having a DRV8811 based PCB that driving a stepper motor which is used to control valve movement. Recently we are seeing some PCB failures. After some debugging and it is found the DRV8811 has been failed due to some reason. This DRV8811 chip failure is confirmed with a low impedance between VMA/VMB (pin 28/15) and GND (pin 7 or pin 21), and a low impedance between VCC (pin 10) and GND (pin 7 or pin 21).
In our design, VCC is 3.3V, VMA/VMB is 24V, Vref is set to about 0.65V and Rsense is 0.22Ohm. This gives a full-scale chopping current of 0.37A and total power consumption of less than 0.3W.
Just wondering what could cause a failure of this chip because it has overcurrent protection and thermal shutdown. But we are seeing a real failure of the chip itself rather than shutdown. Any ideas? Thanks!
Best,
Yuchen