Other Parts Discussed in Thread: DRV2604
What I want to do :
- Store the amplitude of my control
in a register (RTP mode).
- The pulse width in which, the LRA motor
executes this amplitude, which is also
stored in a register.
The 2nd point is not convertible, because the control of the pulse width is realized via the IN pin.
However, the use case provides only the I²C communication to use.
The question is: Which other motor driver can perform this function as required?
I thank you in advance for the helpful comments :)