Hello TEAM
I have 2 question
1) I would like to know if the p/n PDRV8243SDGQQ1 is to be considered fully functional (considering the differences with
the production model) and suitable for use in production.
2) Reading the new version of DRV8243 data sheet SLVSG23B – DECEMBER 2021 – REVISED JULY 2022, I found this note
"The over current protection function does not support direct output (OUT1, OUT2) shorts less than 1 μH above 28 V".
I would like to know if the over current protection function support direct output short less than 1uH above 28V to GND and
if the ITRIP regulation function support direct output (OUT1, OUT2) shorts less than 1 μH above 28 V
Regards
Rodolfo