Other Parts Discussed in Thread: STRIKE
Hi,
I'm considering to use the DRV8343-Q1 in an application that takes place in a 24V system. Page 8 of the datasheet says:
"VM recommended operating condition for electrical characteristic table. Product life time depends on VM voltage. The device is intended for 12–V and 24–V battery automotive system with life-time nominal voltage of 5.5 V - 50 V. The device can be operated during additional overvoltage events as specified in ISO16750-2:2012"
So, can you tell me which overvoltage events the DRV8343-Q1 can withstand regarding the standards ISO 16750-2 and ISO 7637-2? I need to know that because I have to estimate the effort for the input protection for the application.
BR
Tom