Hello
I have a problem about using DRV8353.
While I was driving our motor on approximately 30 Amps, the DRV8353 displayed VDS_HA fault and the motor shut down.
The driving was going on for 5 minutes at 30 Amps. Our Driver Board was overheated. I replaced a new DRV.
I decreased the IDRIVE values from 600 mA to 300 mA and I tried again. The new DRV8353 has burned out one more time.
Now, I can drive the motor without phase A high side, but waveforms of all phase are dramatically bad.
We can share several oscilloscope screenshoot. The figures may not be sequent.